Part Number: ADS1261
Hello,
we are planning to use ADS1261 in our design. we have a requirement to measure 3 sensor outputs using 3 differential channels. By considering various factors like input voltage, reference voltage, no. of channels and cost etc.. we are preferring ADS1261. In our older design we used 3 ADC's to do this operation simultaneously. Below are my questions.
Q.1) Is there a possibility to do the simultaneous sampling of 3 channels using ADS1261 with single start command?
Q.2) If not simultaneous, what is the time required for getting the 3 channel data? for example, if ADS1261 is configured with 50SPS then the time required to do 3 channel's conversion would be 3*20 ms theoretically.
so it require 60ms to get 3 samples. Is my understanding correct?
Please advise.
Thank you.