This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8685: Register Setting Ranges - Question on Table 6

Part Number: ADS8685
Other Parts Discussed in Thread: ADS8695

Customer has pointed out something in the DS for the ADS8685.

Table 6 from p44 says:

- Input Alarm Flags is D[9:7]
- ADC input range is D[7:4]

Both have "7"

But in Table 7, it says:

- ADC input range is D[13:10] (4 bits)

They are wondering if the Input Alarm Flags should be D[9:8] and ADC input range D[8:4]...

I think there was just some miscommunication, but I would just like a second opinion on the register bits in Table 6 and 7 to confirm they are accurate.

Thanks!

Darren