Part Number: ADS54J64
Hello,
Ramp pattern can be selected by register 91h bit 7-4 = 0100.
But, here, what is the ramp pattern exactly?
The ramp pattern consists of 2’s complement code or offset binary code?
If it is 2’s complement code, the pattern start from 1111,1111,1111,1111b and is incremented by 1b every sample period and eventually reached 0111,1111,1111,1111b, then get back to 1111,1111,1111,1111b next and this cycle repeats?
If it is offset binary code, the pattern start from 0000,0000,0000,0000b and is incremented by 1b every sample period and eventually reached 1111,1111,1111,1111b, then get back to 0000,0000,0000,0000b next and this cycle repeats?
Best regards,
K.Hirano