Other Parts Discussed in Thread: UCC27524
Hi everyone.
As I've posted on another thread, we are developing an equipment for process control with a load cell. We need to read values and perform calculations in less than 1ms.
We have developed this circuit that I'm posting here for your kindly review.
Starting with the power management. We will have only one of power source from a 24VDC PSU. So we are using a Synchronous Step-down Voltage Converter(LMR33620ADDA), which seems to be very efficient and has low EMI and low switching noise. Before that we have two LDO, one for AVDD(5V) and other for DVDD(3.3v) which we'll use to supply the MCU and digital supply for ADC1235
Here we are representing the load cell connections
And here we represent the ADC circuit with ADS1235 and UCC27524 for switching the AC Excitation
I would be grateful for any help you are able to provide