Part Number: DAC34SH84
Other Parts Discussed in Thread: DAC3484
Hello,
We are planning to use the DAC34SH84 for a new project.
I am looking for answers to the following questions and will be grateful for your help:
1) How different is the DAC34SH84 from the DAC3484?
2) The data interface supported is up to 750Mbps, so does it mean that each of the four channels can be fed data at this rate?
3) Is there a Xilinx reference design provided? Could you please send me a link
4) Iff my FPGA can support a clock of 750MHz then can I generate signal 750MHz with this chip using IQ modulation?
5) An extension of my previous question: So from the chip I can generate two modulated carriers each 750MHz wide.
6) The data interface is 750Mbps per DAC and since the same 16 bit LVDS interface is fed to two DACs does it mean that the data is 1500Mbps in DDR mode?
7) So I can use a OSERDES from a FPGA to feed data on the 16bit interface
Thanks for your help in understanding the chip,
SM.