Part Number: DAC7760
Hi Ti,
We are using two DAC7760 to capture range of voltages
1. ±5 V (dac7760_circuit attached)
Read dac register form both DAC7760 is not working, SPI read/write timing is matching with datasheet(please refer the attached).
Following are the 24 bit spi write in init sequence
1. 56 0001(init1.jpeg)
2. 01 0001 (init2.png)
3. 55 1002 (init3.png)

Read DAC register sequence
1. channel 1 ±5 V (dac1_read) No data on MISO

2. channel 2 0V to 10V(dac2_read) MISO data not aligned with clock
Channel details:
c1: chip select
c2: MOSI
c3: MISO
c4: clock
Can you help us to solve this?
Regards,
Manoj