Hi,
We are trying to use ADS124S08 to build a high accuracy data acquisition board. We need to make sure that the ADS124S08 is good enough, from the spec the INL is around 1~3 ppm, we are confuse about this INL value. It seem that it is not possible to get this value from production line.
time caculation:
2^24 = 16777216 code,
sample rate = 4000 S/s,
To get each output code of the ADC value, it will take the time around:
16777216 / 4000 / 3600 = 1.1 hours,
So from the calculation above, it seem it's not possible to get this INL value from the poduction line as the test time is too high , I think you can get this from Lab validation, but how do you make sure each ADS124S08 chip from production line have the same value with the one in the Lab?
How can I verify this INL value of this chip before soldering?