Other Parts Discussed in Thread: LMZ10500
Hello,
I would like to use the internal 1.2V reference for external circuits. What is the maximum load current that can be safely supplied?
And can the pin sink current, if so, how much?
I'm asking about sinking current because I would like to make a 1.44V reference with a divider from 3.3V to REFIN. There will be some error introduced by the 3.3V supply voltage but at least this is reduced by the divider ratio ((1.44-1.2)/(3.3-1.2)=0.114). Resistors could be 10k+1.3k, so sink current would be 190uA.
Thanks, Ken