This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Who can help with identification of microchip`s marking?
Part numbers are ADS8343E and ADS8343EB
So, if base on packaging part marking lookup, model ADS8343EB must have this part number:
ADS
B
8343E
But in facts i have this one:
And if base on packaging part marking lookup this correspond ADS8343E
Tell me please is mislabeled or no ?
Or maybe latter B should in another place ? Because judging by the width, the partnumber won't fit
And should look like part number at ADS8343E and ADS8343EB ?
Thanks,
Pavel
Hello,
The images did not make it through, please try attaching them using the "Insert Image" button in the editor.
Our internal systems are showing the same as the publicly available TI part marking lookup tool (link below), and that there should be an extra "B" in the topside marking of the ADS8343EB.
Hello,
You have the "ADS8343EB" material. This can be seen by the large extra "B" in the top left corner of your image. Our internal systems show the "ADS8343E" material does not have this extra "B" in the corner.