Part Number: ADS8688A
Hello Team,
My customer would like to know if it is possible for the pin REFIO to have 2.5v as external reference input or not?
SECTION 8.3.8.2 first paragraph (datasheet) an external 4.096-V reference must be applied at REFIO (pin 5), which becomes an input pin.
Then he is pointing out the next statement that:
"Any low-power, low-drift, or small-size external reference can be used in this mode because the internal buffer is optimally designed to handle the dynamic loading on the REFCAP pin, which is internally connected to the ADC reference input."
Regards,
Renan