Other Parts Discussed in Thread: ADS1271
Hello!
I'm planning to drive multiple ADS1271 by a single 16-bit PIC, using its 2MHz Serial clock to drive both master clock and serial clock of ads1271.
However, upon reading the datasheet, I found these following lines:
For the fSCLK/fCLK ratio of 1, care must be observed that
these signals are not tied together. After Power On, SCLK
remains an output until a few clocks have been received
on the CLK input.
Does it necessarily means that I could not synchronise ADS1271 by connecting a single serial clock from the PIC to both master and serial clock of ads1271?
Shaotong Zhang