Part Number: DAC108S085
Hi,
Customer is using DAC108S085.
The DAC108S085 VCC and VREF1,2, the same 5.0V line of power are used as shown in the schematic.
1. Is there no problem with using the same power supply for VCC and VREF1 and 2?
2. Is it okay to connect VCC and VREF1 and 2 with a different power source?
Are there any additional guidelines for 3.1 and 2 methods?