This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1262: IDAC rotation and temp senser solution support need

Part Number: ADS1262


Dear colleague,

Our customer is evaluating ADS1262, we find an IDAC rotation function in datasheet. It means to change the IDAC connection to output alternately.

So

1. What is the IDAC rotation function? when to use it?

2. In the previous solution, they are using LTC2983+PT1000, precision is ± 0.3°C in 0-100°C, and response is slow. So they plant to use ADS1262+PT1000 to realize that precision is ± 0.1°C in 0-100°C. So ADS1262 is the best choice? or we have a better solution?

Thanks a lot!

Best Regards,

Rock Su