Part Number: DAC3484
Hello,
To be able to use the QMC (quadrature modulation correction) feature in the DAC3484 does the DAC output have to be DC coupled to the IQ modulator or does it also work with AC coupling?
2) It is possible to generate an IF using only a real input (no I and Q, only I centered at the IF). How is it different than using I and Q and using the complex mixer to generate the IF.
Thanks for your help,