Part Number: DAC8775
Hi,
When over temperature condition is occurred, does "SPI operation" work correctly?
Thanks and best regards,
M.HATTORI.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC8775
Hi,
When over temperature condition is occurred, does "SPI operation" work correctly?
Thanks and best regards,
M.HATTORI.
Hi Hattori-san,
SPI operation is not guaranteed when the device is in an over-temperature condition, but it should be able to. The over-temperature alarm will assert when the device temperature is greater than 150°C. It is recommended that the device be configured to take immediate action when this condition is met, such as disabling the DC/DC supplies to reduce power dissipation. The device is also well beyond the specified temperature range at this point.
Thanks,
Paul