Hi, we are thinking about using AFE0064 to detect our current signals with both positive and negative polarities. I found that by applying voltages at pin 56 and pin 57, it is possible to detect both positive and negative currents (Figure 10). I want to ask if it is possible to apply certain voltages at pin 56 and 57, such that Vint_off in Figure 10 is in the middle of REFP and REFM. In this case, the detection ranges for positive and negative currents are equal. If not, what is the limit of Vint_off that I can set? Thank you!