HI Sir
How to clear bit 12 (CRC ERROR) when it generate, could I use firmware skills instead of hardware reset?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Sir
How to clear bit 12 (CRC ERROR) when it generate, could I use firmware skills instead of hardware reset?
Hi Alex,
the CRC_ERR bit should clear automatically when the STATUS register is output as the response. If a CRC error occurs, then the ADS131M04 should output the STATUS register as the response in the following frame. Means in the next following frame you should not see the CRC_ERR bit set anymore unless you had another SPI CRC error.
Let me know if this is not the case then we can dig into it further.
Regards,