Other Parts Discussed in Thread: ADS1235
Hi team!
My customer is having some stability issues with this part - there seems to be too much noise with ADC counts.
The ADS1220 is configured with following parameters:
- Gain => 128
- 50Hz/60Hz filter => on
- 110 samples per second using a one shot conversion command
- Data rate => 175Hz
The ADC is attached to a analog load cell with 2mv/ V sensitivity. The excitation voltage is 5V.
singleshot.xlsxAttached is the spread sheet of test results with 0 weight on loadcell and the schematic.
Following are the register settings:
R0 0x0E ... GAIN 128
R1 0x60 ... DATARATE 175
R2 0x40 ... External reference using dedicated REFP0 and REFN0
R3 0x02 ... DRDY is indicated on DOUT/DRDY
The voltages on signal path and AVDD are:
TP1=5.015V => REFP0
TP2=2.508V => SIG+
TP3=2.508V => SIG-
TP5= 0.000V => REFN0
TP7=5.0174V => AVDD
Please reach out to me internally for the schematic and I can share that with you as well.
Thank you!
Lauren