This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex,
Yes, you can connect the IDACs to any input pin, even one you are using to measure the input channels or use as a VREF input. Table 5 in the ADS1263 datasheet gives a good summary of the pin functions.
One thing to consider is that any filter resistors on those input channels or even trace impedances could cause an error on the reference or input signal measurements, since the current will cause an additional voltage drop across these components. We generally recommend using a separate pin to route the IDAC current through the reference resistor / RTD to avoid these issues.
-Bryan