Part Number: ADS1261
Hi, I have a question about the accuracy of IDAC(MAX-MIN).
The IDAC accuracy is ±4%(Ta -40℃ to +125℃).
However, in the data sheets Figures 42-45, the IDAC accuracy is probably around ±0.7% at all temperatures.
Under what conditions does IDAC accuracy decrease?
I want a constant current of 100uA with an accuracy of 1%.
I am wondering if I can use this IDAC conditionally.