Other Parts Discussed in Thread: ADS1235
Hello guys,
One of my customers is evaluating ADS124S08 for their new weight scale products.
At this moment, they have the following question. Could you please tell me your advice?
Q. Their weight sensor output level is very small. It is about 1V as the maximum even though PGA is set x128.
So they is going to try to use an external reference IC which has 1.024V or 1.25V output to increase effective resolution for the PGA output (about 1V).
Is there any problem or any degraded performance when 1.024V or 1.25V external reference is used instead of 2.5V internal reference?
Your reply would be much appreciated.
Best regards,
Kazuya.