Other Parts Discussed in Thread: ADS1220
Hi team,
We are looking for a new ADC solution below.
1. 16bit
2. 1~2 channel current source input
3. DVDD can be powered with 1.8v.
Could you please help recommend? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Frank,
Here is a link to the Precision ADC parametric search with the following filters applied:
There are 36 options, so if you can provide any more information about what the customer needs we can narrow down the search further to an appropriate ADC.
Also, please note that we don't currently have any ADCs with transimpedance amplifiers built in, but that just means that you will need a small resistor to translate the current to voltage.
-Bryan
Hi Frank,
Thank you for clarifying, I thought you had said "current source input" to mean that you were looking for a current input ADC, since the ADC's integrated current sources would be considered outputs.
If that is the case, then the ADS1220 is the best option, though DVDD min is 2.3V. If you would like to reach out to me offline to discuss the customer's specific needs and use-case, please do so.
-Bryan