Hi Team,
This is customer request, can you please advise:
"
1-) We are getting ADS5463EVM from Texas. This 500 MSPS contains an adc. But we will work with 100 MHz. So adc will work faster than us. But in the adc's datasheet, the clock input sample rate is specified as 20 MSPS to 500 MSPS. In this case, can we adjust the speed of this adc with the CLK that we will apply to ADC according to our 100 MHZ processing speed so that we do not miss data. Otherwise, if ADC works with 500 MSP continuously, we will be able to get 1 data in 5 data of adc, right?
2-) ADC has DRY (data ready) pin and signal. We need to check this pin to get the data. But there is an expression such as "It is recommended to use the DRY signal to capture the output data of the ADS5463" in the datasheet, so if we do not check the DRY signal, can we get the data properly by applying the CLK signal?
"
Thanks in advance
Best Regards
Furkan Sefiloglu