Hi TI team ,
Our new project use two ADS1293 in series for 9-lead ECG application without RLD electrode and find some question as below :
If first ADS1293 AFE Setting LOD_CN (0x06) : 0x14 and second ADS1293 AFE Setting LOD_CN (0x06) : 0x14
9-lead LOD function is workable , but V-lead have noise as shown below :
If first ADS1293 AFE Setting LOD_CN (0x06) : 0x14 and second ADS1293 AFE Setting LOD_CN (0x06) : 0x00
9-lead LOD function is workable , and V-lead have no noise as shown below :
Why the two ADS1293 AFE LOD_CN need to set up different lead off mode ?