This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1148: Clarification

Part Number: ADS1148

Hello Team,

The datasheet indicates of ADS1148 a max data rate of 2Ksps. My customer plan on cycling through the 4 differential inputs.  Am I correct in thinking they can get 500 sps per channel?

Regards,

Renan

  • Hi Renan,

    Check out Table 10 in the ADS1148 datasheet that shows first data conversion time. You can see that the first conversion takes 0.514 ms or 0.578 ms at 2 kSPS depending on how you reset the digital filter, so the resulting effective data rate is slightly <500SPS (0.5 ms) per channel, but it is close.

    -Bryan