Hi everyone ;
Happy new years ,
We will use ADS1292R in single lead mode without RLD ; and we need measure the impedance ( base resistor) between 0Ohms to 1K oHm ; does the non use of RLD effect the performance of the impedance channel ?
is it possible that range from 0 to 1k ?
what does the impedance channel readings give me ? the voltage accross the whole pass of the imedance ( electrodes + protection resistors + base resistor) or it give me the base resistor directly ?
do I need further analysis to find the base resistor ; LPF ?
How does the imedance channel in single lead effect the pace detection too ?
in single lead we use capacitors to block the DC offset with pullup to to RLD 10M with 1uF . we noticed the settle time of the high pass filter is about 14 seconds ; any suggestions here ?
Thank you inadvanced ;