Part Number: DAC8728EVM
We are seeing some things where the DAC8728EVM PCB does NOT agree with the schematic.
For example, for J1, all of the even pins 2-20 are connected to DGND as shown in the schematic for the EVM. For J6 however, none of the even pins 2-32 are connected to DGND even though the schematic shows they should be. We verified this by measuring with a multi-meter in ohms mode. Is the schematic wrong or did the J6 connector just not get routed per the schematic? Which is correct, the schematic or PCB?