Part Number: DAC60004
Hello,
I plan to use some DAC6004 in one of my design.
I will have 4 DACs. All of them will be using the same 2.5V-reference. This reference will be shared with ADCs (for these parts, the accuracy of the reference is extremely important and it must not be influenced by other components). The REFIN input current is critical in my design as it may create a voltage drop (few µV) in the PCB tracks.
I have, thus, several questions regarding the REFIN pin of your DAC.
1) What is the impedance of the REFIN terminal ?
I found two information in the datasheet that seem different :
And :
What is the impedance of the REFIN terminal ? Shouldn't it be 30Kohm/4 as there are 4 buffers in parrallel ? What is the difference between these two values ?
2) Is this impedance really constant ?
This leakage current may not be a problem if it does not change over time and temperature.
So :
- is the REFIN impedance the same no matter the mode (normal mode or power-down mode) ?
- is the REFIN impedance constant over time (no matter the DAC output) ?
- do you have information about the temperature coefficient of this impedance ?
I thank you for your time,
Best regards,
Jean-Baptiste