Part Number: ADS131M08
Hi!
I want to use 3 ADS131M08 to read simultaneous data from the 24 channel (8 channel per ADC) with 1 MCU. After reading the datasheet, I'm not sure if I should do this using 3 different SPI and connecting the SYNC/RESET pin between the 3 ADC to syncronize the reading or if I should use just 1 SPI bus for all 3 ADC.
I need to measure all 24 inputs in 500us max.
Thank you!
Fabiola