Part Number: ADS5463-SP
Hello team,
My customer has a question about single-ended input of ADS5463-SP.
This ADC is a differential input type, but is it possible to use it for a single-ended input signal?
In the data sheet application, a transformer or differential amplifier is used to convert the single-ended input signal to a differential signal, but the customer wants to input the 50Ω single-ended signal to the AIN pin without differentiating it. So if there is a recommended circuit (AIN, AINB, VREF peripheral circuit) for single-ended input, please let me know.
Also, I would appreciate it if you could tell me what kind of difference the AD conversion performance is between single-ended and differential.
Best Regards,
Ryotaro Fukui