Dear all,
Having received the ADS1256 units we ordered, I'm testing one out using a loadcell output (millivolt-range).
Two questions I was wondering about:
1) For the circuit layout, would it be fine to use an external 4 MHz crystal & 18pF capacitors for the XTAL pins (instead of the 7.68 MHz & 18pF capacitors recommended)?
I expect, based on reading the datasheet, that the only change apart from the sampling rate would be a doubling of the analog input impedance.
2) I have never done SPI coding to interface with an external ADC, having till now only used microcontrollers with ADCs already built-in, for data collection.
Can anyone provide Code for an example of how to set ADC register values and acquire ADC data basically? I seem to have read somewhere in the posts that TI also maintains sample code for the ADS1256...
Cheers,
Gamin