This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1118: 14 bits on internal temperature and 16 on thermocouple

Part Number: ADS1118

Hi Guys 

I have a question related to the temperature measurement, on the data sheet al least for the internal temperature sensor into the device it would show as 16 bit conversion, but we only use 14 bit left justified, I do on that way and it works. My question from here is how was calculated the the value 0.03125 to convert the code to temperature using the formula code*0.03125= temp.

Now using a thermocouple we need to consider the 16 bits or 14bits only as the internal temperature sensor. My setup is AIN2_AIN3 as inputs, FSR to 2.048, 8SPS I would like to know how to convert that code to temp