Part Number: AMC7836
Hi team
- The 7836 datasheet only has the load capacity at room temperature, is there a curve for more other temperature range?
- The Datasheet shows that the load capacity of the AMC7836 single-channel DAC is about 40mA. If our 16 DACs all output 40mA (16*40=0.64A) at the same time, will there be any potential problems except that the junction temperature of the chip cannot be exceeded?