This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7953-Q1: SDO answer not two Byte

Part Number: ADS7953-Q1

Hello,

i just confiured the SPI of the ADS7953-Q1 and I am able to read out the messages send by the SDO. I configured the ADS7953-Q1 in automode-1. But it is not possible to read the upcounting channelnrs (4 MSB).

If I watch the SDO signal with the oszillograph it seems to be less than two byte. Do you have an suggestion what is the reason for? 

Thank you for helping

  • Hello,

    What line is the SDO and which line is the SDI?

    Also, this device has a three frame latency. This means that frame 1, is where you tell the device what channel to sample, and then on frame 3 (two frames after) is where the output data asked for in frame 1 is outputted.

    if you are trying to get data for the first 2 frames after power up, then you will not get the data you are expecting.

    image below is from the datasheet of the catalog version

    Regards

    Cynthia