Part Number: DAC71416
Hi,
I am trying to configure DAC71416 I am trying to read Device ID but I am not getting the response, I have attached the schematic and MOSI - yellow line and MISO - blue line output 

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC71416
Hi,
I am trying to configure DAC71416 I am trying to read Device ID but I am not getting the response, I have attached the schematic and MOSI - yellow line and MISO - blue line output 

Hi,
I just want to ask couple questions.
1. Are you facing issue only in read back?
2. Whats the value of reference voltage on the device after power up?
3. Which register are you trying to read back?
4. SDO mode? ( FSDO settings)
Please note that read back requires two SPI frames, first frame SDI will be read command and second frame can be any command.
during the second frame of the SPI, you will get the requested data on SDO.
Can you please post CS, SCLK, SDI & SDO wave forms? In your post why SDI is having some offset ( waveform is centered around zero?)
Regards,
AK
Hi,
1.yes
2.
3.Device ID of DAC71416
4.SDO is enabled.
i am looking for device id in DAC71416. in KEIL software through SPI configuration.
here in this dac we using 24bit. in this 24th bit represent the read/write operation.
23rd bit is 0 for write operation
23rd bit is 1 for read operation.
22nd is dont care
21-16th bit is
Register address. Specifies the register to be accessed during the read or
write operation.
15-0 bit is
Data cycle bits. If a write command, the data cycle bits are the values to be
written to the register with address A[5:0]. If a read command, the data
cycle bits are don't care values.
before accessing the device id we must enable the streaming mode , SDO enable, FSDO enable in SPICONFIG register.
so i am writing
0X03000D;
Then i am reading
0X810000;
This is the main program,that too i puted in while loop
SPIx_EnableSlave();
/*write operation*/
SPIx_Transfer(0x03);//enable spiconfig
SPIx_Transfer(0x00);
SPIx_Transfer(0x0D);// Streaming,sdo,sdo updates at rising edge
SPIx_DisableSlave();
SPIx_EnableSlave();
/*write operation*/
SPIx_Transfer(0x81);//enable device id
SPIx_Transfer(0x00);
SPIx_Transfer(0x00);
SPIx_DisableSlave();
but i am not getting the device id
Hi Sasi,
Can you please share the scope shots of your SPI frame?
Regards,
AK