This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSC2013-Q1: About Power-ON Reset function

Part Number: TSC2013-Q1


Hi,

Please tell me about the Power-On Reset function of TSC2013-Q1.

TSC2013-Q1 has a Power On Reset specification.
Minimum release of the built-in POR is 200 msec.

Customer uses an external reset circuit.
External reset signal is 100msec-300msec accurate
Is it a problem that the internal POR and the external reset pin signal conflict?



Regards,
Yusuke

  • Hello Yusuke-san,

    If the minimum time of 200ms is not met, some unexpected behavior may occur. Although we cannot predict what will happen, the possibility of a latch up may occur. It is best to ensure that the 200ms time is met. 

    Regards,
    Aaron Estrada