Part Number: ADS7052
Other Parts Discussed in Thread: ADS7056
Hello TI member:
I have some questions about the datasheet of ADS7052, could you help me to clarify them ? Thank you !
Q1
The typical INL of ADS7052 is announced about +/- 2 LSB in the spec table, but why Fig.16 seems it can achieve such a great performance about +/- 0.7 LSB ?
Furthermore, Fig.19 shows that INL with temperature through -40°~125° is about +/- 2 LSB, but in Fig20. it shows only +/- 0.7 LSB at 25°C?
Q2
There are two well – known methods to estimate INL ( best-fit & end-point ), which method is recommended or used for data sheet ?
Thank you!
B.R
Chen