Part Number: DAC8760
Hi Team,
We would like to use DAC8760 for “1V to 5V” and “4mA to 20mA”.
We understand that if we use calibration function, “The gain register must be programmed to a value of 0x8000 to achieve the default gain of 1” .
When, we set CODE=FFFFh, analog outputs(voltage and current) are 5V(max) and 20mA(max) even if the gain resister is more than 0x8000.
Is my understanding correct?
Regards,
Hide