This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131A02: Buffer amp bandwidth

Part Number: ADS131A02
Other Parts Discussed in Thread: THS4561

Hello Support team,

I have a question about the buffer amplifier at front of ASD131A02.
I will use ADS131A02 under the following conditions.
Fmod (operating clock frequency) = 4.096MHz
OSD (Oversampling Rate) = 256
ODR (output data rate) = 16kHz
Is it correct to think that there is no problem if the bandwidth of the amplifier used in the AD driver circuit in the previous stage is higher than Fmod (4.096MHz)?
If you have any recommended buffer amps, please let me know.

Best Regards,
Hirokazu Takahashi

  • Hello Takahashi-san,

    Thank you for your post. 

    Depending on the application requirements, the amplifier bandwidth should be at least 4x-10x greater than the modulator sampling frequency. This assumes that the amplifier is used in a unity-gain configuration. If the driver stage is configured for gain > 1 V/V, more bandwidth may be required. 

    The input R-C charge-bucket filter (similar to a SAR ADC circuit) also helps to provide charge to the internal sampling capacitors. The amplifier circuit should be tested with this R-C load to ensure amplifier stability.

    The ADS131A02 uses two internal clock dividers to generate the modulator frequency. If the amplifier circuit is designed for 4.096 MHz (max fmod), the circuit will still work well for slower fmod frequencies. 

    In the past, we have used fully-differential amplifiers (FDAs) like the THS4561 for unbuffered delta-sigma ADC inputs. The input impedance is not very high, so a separate high-impedance buffer might be necessary at the FDA inputs.

    Regards,

  • Hello Ryan-san

    Thanks for your prompt reply.
    The base bandwidth of input signal is DC for our application and the buffer amp gain will be x1.
    We think noise performance is better with higher fmod.
    Is it necessary to set the bandwidth of buffer amp at least 4x-10x greater than fmod in that case?
    If so, may I ask about the detail reason?

    Best Regards,
    Hirokazu Takahashi

  • Hello Takahashi-san,

    The amplifier bandwidth requirement is based on the transient voltage settling that happens in the beginning of each modulator period. You can think of this as the acquisition time in a SAR ADC sample-and-hold circuit. 

    What is the source of the DC voltage that you are measuring? In some applications, we see customers measuring these types of signals without much signal conditioning, so it really depends on the signal characteristics and target accuracy.

    Regards,

  • Hello Ryan-san

    Thanks for your support.
    The application is battery tester. So DC voltage source is battery.

    Best Regards,
    Hirokazu Takahashi

  • Hello Ryan-san

    Do you have any update for your advice at the battery source?

    Best Regards,
    Hirokazu Takahashi

  • Hi Takahasi-san,

    I hope our discussion via email was helpful. I'm posting the TI Reference Design here for everyone's benefit before closing the thread.

    TIDA-01040 Battery Tester Reference Design for High Current Applications

    Design Guide

    TIDA-01040 schematic

     


    Best regards,