This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS124S08: Gain/Offset Error and Drift Calculation Question

Part Number: ADS124S08

I was hoping for some confirmation for the TUE calculation.

ADS124S08 DS specifies the following, for full-temp, PGA = enabled and Gain = 1~8
(Convert all to voltages in next step)

Error Sources (MAX) per Datasheet
Gain Error 120 PPM
Gain Error Drift 4 PPM/℃
Offset Error 120/GAIN = 30 uV
Offset Error Drift 200 nV/℃
INL 15 PPMfsr

My question is, for the TUE calculations you need to know the FSR.
Assuming the reference to be 1.5V, the FSR = ±VREF / GAIN, right?
So with GAIN = 4, the FSR is ±1.5V/4 = ±0.375V = 0.75V

Using 0.75V as FSR to calculate the TUE gives...

Error Sources (MAX) converted to voltage
Gain Error 0.000090000 V
Gain Error Drift 0.000150000 V
Offset Error 0.0000300 V
Offset Error Drift 0.00001 V
INL 0.00001125 V

Then we add the errors to separate into Gain, Offset, and INL

Total Gain Error 0.000240 V
Total Offset Error 0.00004 V
INL 0.00001125 V

Then we calculate TUE (sum-of-squares)

TUE 0.00024357 V

Am I doing this correctly to calculate worst-case TUE?

Thanks
Darren