Part Number: ADC12DL3200
Hello E2E,
I have some questions about the power sequence of ADC12DL3200 on page 131 in datasheet.
The power sequencing requirement is VA19 ≥ Vx11.
What is the impact if we don't follow the rule?
May it damage the device?
The PG outputs and EN inputs of the regulators can be used to achieve the power-up sequencing requirement.
Can it also be achieved during power-down?
Supply Current : IVA19 = 1300mA > IVA11 = 700mA
The VA19 voltage may drop faster than VA11 during power-down.
Does VA11 need additional protection?
Sincerely,
IT Hung