This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC70504EVM: Reason for capacitor connected to CS input

Part Number: DAC70504EVM

Hi I would like to know why on the eval board, there is a 560pF capacitor on the CS input of the DAC. IT's the only spi interface input that has that. Connecting this input to an FPGA is showing considerably slow down in reaching required voltage on the CS input for properly operating the spi interface

Thanks

Amish