Part Number: SM73201
Hi,
i’m using the ADC SM73201 as in the picture below.
I need some clarification:
-
the VIO voltage is referred only at the SPI signals and it doesn’t affect the voltage input? So if I connect the 3.3V voltage, the SPI signals work at 3.3V. Is it right?
-
I have a differential signal, whose each signal as a voltage range between 0.5V and 4.5V. In other words I have a maximum differential signal of 4V and an input common mode of 2.5V. If I use a VREF=4.096V and a VA=5V, it should work well since the single input voltage is referred to VA and the differential value is referred to VREF?