Part Number: ADS125H02
Hi Bryan-san
If AIN0 = 0V, 1V, and 2V are applied with the following settings, what is the correct answer for the converted values of each voltage?
H VDD = + 15V, HVSS = -15V, AIN0 / 1 = 0-10V, AINCOM = GND
Connect to and set MUX [2..0] = 011b and GAIN [3..0] = 0010b.
-yamamoto