HI,
We are planning to interface ADS7128 for our application where we have below query, Require your feedback to freeze the design architecture:
1) Is it possible to configure interrupt/Alert whenever there is change in State for the digital input pins?
2) Is it possible to provide an specific PWM (10% to 100% duty cycle) signal through a digital Output Pin?
3) We require 2 ADC channel to be used to check the value and whenever they are below threshold it should provide interrupt/alert to host.
- Also we require two digital input of switch-button, which should provide interrupt whenever the switch/button is pressed.
- We require 2 Digital output pins, 1 with PWM functioanlity and 1 with simple enable - disable logic.
Awaiting your valuable feedback.
Thanks,