Other Parts Discussed in Thread: ADS8555, ADS8556
Hey team,
I had a quick question come up while trying to find a part that meets a customer's needs. I think that the ADS8686S seems like the best fit based on the below requirements, but the issue is their input from a pressure transducer appears to have outputs not referenced to the power supply. Can the input for the ADS be configured as a pseudo differential input?
Requirements are as follows:
Architecture |
Number of Bits |
Sampling Rate/Sec |
Number of Inputs |
Input Type |
Data Interface |
Reference Type |
Supply Voltage |
Throughput |
Features |
SAR |
16 |
1M |
6 |
Fully Diff |
SPI |
Int / Ext |
Single supply (5V) |
1MSPS |
Simultaneous Sampling |
Thanks for the advice,
Cameron