Hello. I'd like some clarification of a couple of timing parameters. We are using the ADS1278 as follows: frame sync mode, high speed mode, TDM, IOVDD=DVDD=1.8 V, tCLK=32 ns. I see from the datasheet that the output propagaion delays tDOPD and tMSBPD change with DVDD. My question is what happens if IOVDD changes? Does Note 6 beneath the Frame Sync spec table on page 9 hold for an IOVDD of 1.8 V instead of 3.3 V? Will my configuration result in output delays of 25 or 31 ns? Thanks.