This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Respiration issue

Part Number: ADS1298R


Hi Ti teams,

According to the Hardware spec. & register setting  of ADS1298R, the waveform of respiratory isADS1298R respiration issue.docxADS1298R respiration issue.docxn’t displayed.

The attached file is Hardware circuit diagram & the register settings as followed:

ADS1298R

16h:0xF6

17h:0x22

How can we set the register or revise the hardware to fix respiratory waveform issue ?ADS1298R respiration issue.docx

  • Hi Jam,

    Thanks for the post.

    The respiration schematic looks fine. Are you testing the respiration with a patience simulator? Can you also provide the full device register settings for our reference? Is it possible for you to bypass the two analog switches in the respiration path for testing purposes?

    Thanks.

    -TC

  • Hi Tc,

    Thanks for reply. The respiration simulator FLUKE PROSIM-8 was used with this project, and the ADS1298R register table refer to below:

    Register    Value
    0x01        0x85
    0x02        0x10
    0x03        0xCC
    0x04        0xEF
    0x05        0x40
    0x06        0x40
    0x07        0x40
    0x08        0x40
    0x09        0x40
    0x0A        0x40
    0x0B        0x40
    0x0C        0x40
    0x0D        0x0A
    0x0E        0x0A
    0x0F        0xFF
    0x10        0xFF
    0x11        0x00
    0x12        0x00
    0x13        0x00
    0x14        0x1F
    0x15        0x09
    0x16        0xF6
    0x17        0x22
    0x18        0x0B
    0x19        0xD6

    Thanks.

    Jam

  • Hi Jam,

    Thanks for the register information. Please let me take a look and get back to you.

    Thanks.

    -TC

  • Hi TC,

    Is there any update information?

    Thanks.

    Jam