Part Number: ADS1262EVM-PDK
Hi,
I'm trying to use the ADS1262EVM-PDK to measure the output of a photodiode sensor and circuit. I have the output of the sensor circuit attached to IN0 and the mux setup via the attached image, but I keep getting a PGARAIL_N error. My understand of this is that it may be caused by my sensor output being very close to ground (I measured it at about 1.5mV, which is expected when not exposed to the target spectrum) and that by using the bias voltage on AINCOM, it would offset the voltage into the correct range, but it instead seems to drop the voltage to -2.5V instead, which doesn't seem correct and still causes the error. Is there a different way this should be configured to support readings like this?