I am trying to understand the proper reference setups for various topologies with the ADS124S08. Using the "Basic Guide to..." documentation, datasheets, etc, I have kind of summarized the main design points below. Is there anything else you could add, or correct if I am mistaken?
For an RTD setup...
- A high-side reference can eliminate the IDAC mismatch issue, but because IDAC1 has to go through the reference resistor then to the RTD element, it means you need a MUX if you want to measure more than a single RTD (or else you need multiple expensive reference resistors)
- A low-side reference solves the above problem, but IDAC mismatch errors could be a concern (gain error). Swapping the IDAC sources and taking two measurements, and averaging the codes, could help cancel that mismatch, but at the cost of more processing time.
For Thermocouple setup:
- If using a reference resistor for a thermocouple setup, the IDAC accuracy results in a pretty large gain error. This is because the measurement is not ratiometric.
So for a thermocouple, it is not recommended to use a reference resistor? Instead, it is recommended to use the internal, or external, voltage reference?
- What kind of typical reference voltage accuracy needs do you see for thermocouple applications? Do you recommend the internal reference voltage? (soldering can create slight deformations in the silicon (metal expanding/contracting) which can shift the internal reference voltage, whereas external references are centered in the center of a package and are more immune to this)
For Thermistor setup:
A thermistor setup is similar to a two-wire RTD setup, so do the above high/low side reference concerns apply? I believe they do.
When calculating the error, is there a recommended way to calculate the max/min/typical errors?
If we take the RTD for example, if you calculate the worst-case error from the following:
- Worst case reference resistor ΔΩ over accuracy/drift
- Worst case IDAC mismatch over accuracy/drift
- Worst case lead-wire resistance over accuracy/drift
- Worst case input bias currents
- Worst case ADC internal errors (gain / offset / INL) over accuracy/drift
You end up with a compounded, unrealistic, completely hypothetical worst-case result.
Where could you give-in and use the typical error values in the calculation, and still see most production units passing customer ship-out testing?
I mean, could you use the max/min IDAC, and max/min reference resistor, coupled with the typical ADC internal errors, and be relatively well-off?
Thanks,
Darren